Hi expert,
My customer used BQ76952 and they want to check power on sequence for the system.
Our current power-on sequence is:
AFE is powered on -> MCU is powered on -> MCU communicates to put AFE into shutdown mode -> Pull TS2 low to wake up AFE -> Send SET_CFGUPDATE for the first time, and you can read it multiple times. Bit0 in BatteryStatus is 1, and you can configure data normally and exit EXIT_CFGUPDATE; when you send the SET_CFGUPDATE command later, you can read that bit0 in BatteryStatus is 0 after multiple reads, and you cannot enter SET_CFGUPDATE mode.
Want to confirm:
1. SET_CFGUPDATE——Is it only valid for the first time, and subsequent configurations need to enter shutdown mode first;
2. When AFE is powered on for the first time, it must enter shutdown first. After waking up, can it be used normally?
BR
Emma