Dears:
Customer want to test UCC5870-Q1 function without SPI, As MCU is not ready, they want to test it in default value. Could you please help check if it can work ? Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dears:
Customer want to test UCC5870-Q1 function without SPI, As MCU is not ready, they want to test it in default value. Could you please help check if it can work ? Thanks.
Hi haiwen,
UCC5870-Q1 cannot function without SPI. I recommend using our TI EVM and the GUI. This would be the easiest way to test the functionality of the device.
Regards,
Akshat