This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5041A: Can LM5041B be used as alternative

Part Number: LM5041A
Other Parts Discussed in Thread: LM5041B,

Hi Team,

My customer is currently using LM5041A in their design and are facing shortages. They are trying to use our LM5041B, but are facing issues in their testing. Below is their feedback:

For B every time when the module turn off, buck drive is low, the bus line has energy left. When next turn on comes quickly,

PUSH-PULL MOS will open with 50% duty to endure the bus energy discharge. This will result in the breakdown of PUSH-PULL MOSFet.

We found this failure at frequent on/off.

Is there anthing that can be done for them to use the B version instead?

Thanks!

BR,

Alfred