Other Parts Discussed in Thread: TPS92692
hello, i have one question about the TPS92692 ,
When i use the TPS92692 buck boost cc MODE, I test the LED output current wave .
i did not use the PWM dimming.
LED output current wave as following:
the output current is not straight and fluctuates up and down , the max value is 480mA,the min value is 400mA, why is this happening ?
and i used the dither frequency, i found that if i do not use the dither frequency function, the output current will become a straight line, could you help explain this for me ?