Other Parts Discussed in Thread: BQ33110
Hello BQTeam,
I have some difficulties to configure the BQ34110 gauge. I use a 3S NiMH battery pack.
When I read the voltage with voltage() command, that don’t return the good voltage : 22800 mV instead of 3320 mV.
Moreover, the batterystatus stays at 0x00 even with a negative current.
I attached the gg file. Can you verify it please ?
To configure the flash, i use the following steps :
- CAL_TOGGLE (0x002d)
- Write all flash datas
- RESET (0x0041)
- CAL_TOGGLE (0x002d)
Is it the good method ? i work on STM32 and i don’t have the demo board yet.
Thanks and best regards,