Other Parts Discussed in Thread: TPS25750,
Hi.
I am designing a PCB using the TPS25750 and BQ25792. This PCB must support products that have 1, 2 or 4 cells battery pack.
I use a host processor. The host processor will load the configuration patch file into the TPS25750 through i2C, the TPS25750 in turn programs the BQ25792.
I would like to use the same host firmware, where the host processor reads some inputs to know how many cells that are in the system.
I do not want to have 3 different patch files that need to be loaded depending on the number of cells.
What is the best practice to achieve this?
I am considering to use the I2Cw 4CC command to reprogram the BQ25792, but is there perhaps a more straightforward approach?
Thanks for helping!
Jan