Part Number: TPS55340-EP
Other Parts Discussed in Thread: TPS55340, LM5157, LM5155
I used the TPS55340 before, but the internal Fets seem to handle only up to 5A. I need a 8A solution.
- Would you have a recommendation for an 8A similar part?
- Or, could I use two TPS55340 in combination for a higher power , (they should handle 10A in parallel) Would that be a recommended implementation?