Part Number: BQ76952
Hi
I have a query need your help.
When capacitor C1013 is short-circuited or resistor R1013 is open-circuited, can BQ76952 recognize it and what is the impact?

Waiting for your reply.
Thanks
Star
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Star,
If the capacitor is shorted, the device would read that the current is ~0mA at all times.
If the resistor on SRP is open circuit, then the pin voltage would float and the device could read that as anything.
Regards,
Max Verboncoeur