Hi,
we suspect that the SM-Bus data traffic of the bqWizard compromizes the accuracy of the transmitted data due to too much processor load.
We discharged the same pack twice, first time with the bqWizard logging away heaps of data, the second time the pack discharged without bqWizard. Both times we measured the delivered charge externally. There was a difference of 150mAh.
Also we discovered strange readings of the bqWizard, which should have triggered error messages from the pack, but the pack behaved just fine.
Is there a limit on SM-Bus data traffic to ensure the processor is able to perfom correctly.
Kind regards, Heye