Other Parts Discussed in Thread: BQ25756
Dear all,
Would it be possible to use BQ24800 to replace LTC3350 for supercap management?
Here you can find more details about the application we are interested to:
- input voltage: 12V
- Supercap configuration: 4 supercap of 2.5V in series (10V in total)
- Desidered functionality:
- Superdiode configuration to provide the 12V of the input to the system
- Buck mode to charge the supercap
- Boost mode to provide the 12V to the system, taking the energy from supercap, in the condition of absence of 12V as input
- It would be nice if the IC (BQ24800) is able to handle the change of the operating mode standalone (without having to set the buck/boost mode through the I2C interface)
- It is ok to configure the BQ24800 internal parameters (such as the battery overvoltage) through the I2C interface (in LTC3350 everything is configurable through resistances)
In case you think BQ24800 is not the right IC for this application, can you suggest a different IC to perform the desidered functionality
Let me know if you need further information
Best regards
Alessandro