Part Number: TPS23861
Other Parts Discussed in Thread: TPS23881, TPS23882
TPS23861 part is only compliant with IEEE 802.3at. Do you have any PSE controllers that are compatible with IEEE 802.3bg as well?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Saurabh,
IEEE802.3bg is a Ethernet PHY standard, I believe you are referring to IEEE802.3bt which is the follow on to IEEE802.3at!
Assuming IEEE802.3bt compliance we have the following devices currently available:
TPS23881: IEEE802.3bt compliant Type-4 4-pair 8-channel compliant device
TPS23882: IEEE802.3bt compliant Type-3 2-pair 8-channel compliant device
TPS23882B1: IEEE802.3bt compliant Type-3 2-pair 8-channel compliant device with autonomous mode (no host control needed)
Regards,
Brandon