Other Parts Discussed in Thread: , BQ25895M
Hello,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Hi Stuart,
Thank you for reaching out via E2E. On the BQ25890 and BQ25890H HVDCP and MaxCharge functions need to be disabled in REG02 before the USB input is connected to prevent the charger IC from performing a handshake and negotiating to 9V. Therefore to ensure the device never operated with 9V input you would need to modify bits 2 and 3 in REG02 when being powered from the battery only because these functions are default enabled.
To simplify your design you will ideally want these bits in REG02 to be default set to disabled state. This is the case on the BQ25895M device, which is an IC from the same product family and has the same pin out as the BQ25890.
Please let me know if you have any additional questions.
Best Regards,
Garrett
Hi Garrett,
This is what I tried to do but to no avail. Setting Reg02 to value 0X40 produces the same result. The battery is always connected and I remove and replace the USB cable. before and after programming, to check.
Hi Stuart,
To confirm the theory of operation: If I disable the HVEN and MaxC bits then it should never negotiate anything above 5V?
This is correct. With those two bits set to disabled state the BQ25890 will not attempt to negotiate a voltage above 5V. You do not need to disable the handshake process entirely.
Referring to the figure included below taken from page 17 of the BQ25890H datasheet you can see that disabling MaxCharge and HVDCP will remove the adjustable high voltage adapter handshake block from the detection scheme. The D+/D- detection will still work to detect and set different current limits without requesting a voltage increase.
I also have a few questions regarding the testing you are performing to help with debug.
-How are you connecting the CC pins on your USB type C since they cannot connect to the BQ25890 device?
-If you take a waveform of VBUS input power up do you observe VBUS initially at 5V before it steps up to 9V or does it start up directly at 9V?
-When you set REG02 = 0x40 have you confirmed the device will read back a value of 0x40 from REG02 after configuration and do you have the watchdog disabled [REG07 bits 5:4]?
Best Regards,
Garrett