This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS22950LEVM: TPS22950L - Does the TPS22950L have "Reverse Current Blocking" Functionality?

Part Number: TPS22950LEVM


PART: TPS22950L 

Note the Support Page does not have an option for the TPS22950L so I had to Select TPS22950LEVM as the Part in Question. 

-------------------

Datasheet: TPS22950x 5.5-V, 3.2-A, 34-mΩ Adjustable Current Limited Load Switch datasheet (Rev. B) (ti.com)

Does the TPS22950L have "Reverse Current Blocking" Functionality?

I look Forward to Hearing a Response. 

-------------------

  • Hi James,

    Welcome to e2e!

    The TPS22950L does not have Reverse Current Blocking - please see the table below from Section 5 of the data sheet.

    Thanks for the comment about TPS22950L not being an option for the support page - typically, only "Generic Part Numbers" (seen on product pages f.e. here or at the headers of data sheets) are provided as an option, then any device variant in question is specified in the query. However, I don't think there will be any confusion if you choose to continue to use the device/variant EVM as the part number if there is one.

    Thanks,

    Patrick