Hi, TI expert
A customer is looking for an OCP IC that supports USB OTG.
If there are any ICs that support the following specs among Current Limit IC or OCP IC, please recommend them.
1. From IC INPUT to OUTPUT direction:
- IC capable of setting the Current Limit to 2A
- Input Voltage: 3.6V~15V
2. From IC OUTPUT to INPUT direction:
- It doesn’t matter if you don’t have the Current Limit function.
Please check. Thank you.