This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSF12C3: 3 phase AC input range?

Part Number: TPSF12C3


Hi team,

Does the customer want to know the TPSF12C3 what is max AC input?

customer spec is 180VAC~528VAC.

But looking at it from another view
Is it possible to use the same inductor size but reduce the number of turns and increase the wire diameter to improve efficiency? thanks