Other Parts Discussed in Thread: TIDA-00779
Hello,
I tried to find an answer on the internet but wasn’t able to. So here I am !
I was trying to find a way to supply my ucc28180 and a convenient way would be to use a bootstrap from the main line. However, it is mentionned in the datasheet (tldr: you can’t):
The TIDA-00779 design requires an external bias supply to power the UCC28180 PFC controller
UCC27531D gate driver, and relay, which is used to shunt the inrush current limiting resistor.
TI recommends powering these devices from a regulated auxiliary supply. These devices are not intended
to be used from a bootstrap bias supply. A bootstrap bias supply is fed from the input high voltage through
a resistor with sufficient capacitance on the VCC pin to hold the voltage on the VCC pin until the current
can be supplied from a bias winding on the boost inductor.
The UCC28180 has a UVLO of 11.5 V and the UCC27531D has a UVLO of 4.5 V, whereas the minimum
voltage required to turn on the relay is 9.6 V (for a 12-V relay), so the bias voltage for board operation
must be ≥ 12 V. The total current required for these devices is approximately 55 mA
(TIDUBE1C)
Could you help me please to understand why ? I suspect a question of power dissipation through the bootstrap components or maybe a question of voltage stability ?
Thank you for your time.
Benjamin