While I have generally had a good experience with this device and its datasheet, I am seeing some large inrush currents on turn-on (which I realize will also be influenced by capacitance on my design) as well as somewhat excessive output ringing. I was hoping to mitigate this by adjusting the soft-start capacitance and adjusting how the turn-on enable signal is handled.
1) The published documentation is not exactly the most verbose regarding details on the soft start function. All that is mentioned is that TI recommends a 100 nF soft-start cap for a certain start-up load current and there is no further discussion. The design examples at the end of the datasheet only say to use the 100 nF value and do not go into any detail. Can anyone provide more knowledge regarding the soft-start behavior for this device? Is there a limit to the maximum capacitance that can be applied to this pin?
2) I am interested in playing with some turn-on delay using a low pass network with the EN pin function -- are there any issues with a slow- rising signal on the EN pin?
Thanks for any insights.