This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS3899-Q1: Negative-going input threshold for adjustable sense threshold version

Part Number: TPS3899-Q1

Are there minimum and maximum values for the Negative-going input threshold for adjustable sense threshold TPS3899DL01DSERQ1?  

The datasheet only specifies a typical value, which does not support calculation of upper and lower bounds for voltage trip point.

  • Hi Amy,

    The min and max can be calculated based off of the Negative-going input threshold accuracy(outlined in image below as well as in electrical characteristics table). In your case the minimum = 0.505 * 0.975 = 0.492 V (Min) and the maximum = 0.505 * 1.025 = 0.517V (Max)

    Thanks,
    Joshua