This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ79656EVM-021: TSREF pin isn't HIGH

Part Number: BQ79656EVM-021

I'm using BQ79656EVM-021 and BQ79600EVM-030 (Bridge evaluation board) 

BQ79656EVM-021 evaluation board is connected with  BQ79600EVM-030 on Daisy Chain protocol

Software - BQAutoEval

I want to Read the Temperature by NTC which is mounted on PCB it self(BQ79656EVM-021 ), for that enable the TSREF_EN bit in CONTROL 2 register,

Now my problem is TSREF pin isn't high, 

kindly let me know what more i need to do to make it work.

Thanks

  • Hello,

    Did you properly wakeup and auto address the devices to make sure they are on and communicating? You must do this step before doing any register writes. I would recommend using the scripting feature in the GUI as well do write the data manually.

    Thanks,
    Chase