dears,
my customer is testing the OCC protection of BQ76952 on their PCBA.
when the OCC protection occurs, the CHG FET was disabled and the customer MCU identified the fault in 10~120ms when it happened, then they sent FET_CONTROL() to force CHG FET to keep disabled, but when the OCC protection got recovered after the delay time, the CHG FET got enabled even though the MCU had already sent FET_CONTROL() to the device, then the customer sent the FET_CONTROL() to disable CHG FET again, it then got disabled by the command.
the sch, gg file are attached FYI. please help to have a look.
thanks!