Hello,
I am designing a pcb using the LMG1210. In the recommended layout and footprint sections of the datasheet, there are thermall vias under the thermal pads. Is it ok to use 0.25mm (not filled) vias under the thermal pads? I am afraid that solderpaste might leak during reflow, leading to worse thermall dissipation, compared to not having vias underneath. Do you have any experience or recomendations on this aspect?
p.s. the PCB technology I have to use doesen't permit tented,filled or smaller vias
Kind Regards,
Vasileios