This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76952: Current Sense Resister Signal to Noise

Part Number: BQ76952


Hi! 

We're seeing about 120mV of peak-to-peak noise across our .1mOhm current sense resistor (WSLP5931L1000FEA 1% tolerance, +300ppm/ºC). We're trying to figure out how it could be possible to get an accurate current measurement in this situation. 

What is a typical sense resistor noise level for successful circuits using the BQ76952?  

For example, since 1 amp across a .1mOhm resistor is .1mV, our signal to noise level is 1:1000. How could we expect to measure 1amp or 10amps or even 100amps.  Even if we used a 1mOhm sense resistor (which is used in the example circuit in the data sheet) 1amp would be deep in the noise floor. 

Is the calibration effective enough to make up for this extreme of a signal-to-noise ratio?  Is there anything else we're missing? 

We've done our best to minimize the noise by putting the sense resistor on a separate board in a metal enclosure. And we've added and experimented with multiple filter capacitors.   

We're considering trying to integrate a hall effect sensor to replace the sense resistor. Would a hall effect sensor be more likely to measure a wide range of currents accurately? Do many manufacturers choose hall effect sensors over sense resistors?    

Thanks for any help!

   

  • Hi Coco,

    120mV is a lot of noise for the sense resistor. Are you seeing this noise in the current readings of the device or are you measuring it directly on the sense resistor?

    Also, have you tried probing around the current loop of the battery to see where this noise might be coming from and if it is present elsewhere?

    Regards,

    Max Verboncoeur

  • Hi Max, 

    We're measuring the sense resistor (and it's filter circuit) on an oscilloscope. But we're also seeing the noise in the BQ's current readings. 

    We've followed the current calibration procedure, but settings for Board Offset don't appear to have any effect on the current readings. 

    Thanks for your help. 

  • Hi Coco,

    Do you know what the source of the noise is? Also, what is the frequency of the noise, and can you share the scope captures? It may be better to measure from the SRP and SRN pins since it is filtered by the RC filters at that point.

    Regards,

    Max Verboncoeur