This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76952: BQ76952 NTC accuracy

Part Number: BQ76952


Hi

According to the RTC resistance table of NTC, the maximum temperature error of the model parameters is more than 2°C.

When the model parameters are actually written into the AFE, the maximum error measured is more than 2°C. When use a microcontroller for sampling, the temperature error can be about 0.5°C.

NTC.rar

Does it normal?

Waiting for your reply.

Thanks

Star