This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62088A: Min On-Time, etc.

Part Number: TPS62088A
Other Parts Discussed in Thread: TPS62088,

Hello,

I have two questions about TPS62088A (forced PWM).

  • What's the minimum on-time of the TPS62088A?
  • The WEBENCH Power Designer tool shows a switching frequency result of about 4.2 MHz with TPS62088 (PFM/PWM) while the result is 2.17 MHz with TPS62088A (forced PWM) under the following condition. The TPS62088A's result is clearly strange from the data sheet specs, too. Is something wrong with the WEBENCH simulation?
    • Conditions
      • Input voltage: 3.3 V
      • Output: 0.9 V/1.8 A

Best regards,
Shinichi Yokota