Other Parts Discussed in Thread: UCC28056,
Hello, I'm developing a PFC interleaved transition mode. I know that some non-interleaved transition mode PFC controllers allow you to use an inductor without an auxiliary winding. For example UCC28056 as also discussed in the SLUA920B application note. I wanted to ask you if it is also possible to use inductors without auxiliary winding in interleaved transition mode PFCs. This is really important for my company. Do you have a controller to suggest? In case the interleaved controllers do not have this function there are non-interleaved controllers
with this function (such as UCC28056) which can however be synchronized with another controller of the same type
in order to obtain an interleaved ? Thank you