In order to permanently maintain a 100% duty cycle for OUT, is it OK to connect the "Delay Adjust" pin directly to ground such that it always stays below the 2.6V threshold? We have found that a large enough resistor on the "Duty Cycle Adj" pin also gives us 100% but the datasheet suggests there may be a 90 to 95% max limit. Thanks.