This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS3760: Correct part numbers for 12.0 and 12.4 volt detectors

Part Number: TPS3760

Looking for voltage detectors, 12.0 and 12.4 volts.  having trouble coming up with correct part numbers in tps3760 or maybe I'm not understanding something about the numbering system.  Can I get some help, please.

Thanks

  • Hi Justin, 

    We do have limited variants of TPS3760 release at the moment. The 12V and 12.4V variants are currently not released.

    If your design can accommodate, we do have the adjustable variant of the TPS3760 available. For the adjustable variants, you will need voltage dividers to get the threshold that you need. 

    TPS3760A012DYYR Under voltage detection

    TPS3760E012DYYR Over voltage detection

    For your question, the third and fourth X will be A4 or A5 for the threshold that you need. 

    Jesse