Other Parts Discussed in Thread: LM25148
Hi, I'm designing a power supply system for a High brigtness Led display.
My requirements are 3.5V 40A wich i though would fit a LM25149 in dual phase arangement,
But in the datasheet, the examples scare me a bit, always showing a 20A output, even for a dual phase design (the component is supposed to be able to handle 30A on its own already)
Do you have any part suggestions for such a design ?
Detailed requirements:
-> passive cooling (radiator ok)
-> atleast 30A sustained load and handle 40A for a few seconds
-> input voltage : from 12 to 20-25V
-> Active EMI filtering is a plus but not a requirement
Thank you,
Nalco