Dear supporter,
LM7310 showed how to use 2 different power in parallel.
we have a further request to provide current from both power rail. for example, power 1 is 5.1V from typeC port and power 2 is 5V from typeA.
the current is not enough from either port, so we need they provide current at same time.
Q1:dose it work fine if we put balast resistor in both output. like below
Q2: if the power 1 and power 2 are step down from 5V to 3.8V with bucks, dose balast resistor work ok? will it cause bucks abnormal ?
Q3: LM7310 quencient current is high, any other diode with low Iq?