Other Parts Discussed in Thread: BQ24610, TPS61376
Hello guys,
One of my customers is looking for a DCDC boost converter IC which has VINDCM(Input Voltage Dynamic Power Management) function.
The customer wants to build a product like the following.
Input: 5V(connected to USB port of PC or mobile battery by USB type-A cable)
Output: 6.5V/2A(Max)
They know that it is not possible to realize 6.5V/2.5A(Max) output from USB type-A.
But the requirements is come from their end customer.
So they are looking for a DCDC boost converter IC which has VINDCM(Input Voltage Dynamic Power Management) function though output current is reduced to less than 1A.
Do you have any boost converter which has such function?
Or is their any way to realize the function using TPS61033 with any other IC?
Your reply would be much appreciated.
Best regards,
Kazuya.