Hi team,
This is FAE Jimmy local in Taiwan. this LDO is using at LF loop's power. My customer test the condition Vin lower than 5.1V at sleep mode and get the higher quiescent current.
when they test the Vin above 5.1V the system totally quiescent current is around 1.81mA. when they test the Vin under 5.1V the system totally quiescent current will be around 37.2mA. since the system is in sleep mode that only remove this LDO the quiescent current will back to 1.8mA. and I also check the LDO output's device is no working(in sleep mode). so If I need to explain this situation to customer would need the data about LDO's output current when it Vin lower than 5V. do we have similar test result like Output Voltage vs Output current as below datasheet Figure 3. Output Voltage vs Input Voltage?
BR,
Jimmy