This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Inquire about inverter solutions.

Hi

My customer wants to develop inverters with the following specifications.
Please recommend a solution.

-SPEC-

Input: DC 72~84V

Output: AC 220V(4KW)

Voltage Conversion: DC 72~84V =>DC 400V => AC 220V

Thanks 

  • David,

    You can search the TI Reference Design Library here. Most all TI inverter reference designs are using or interfacing to C2000 microcontrollers so you may want to include this in your search. Otherwise, could you please submit a new E2E thread with a TI part number in the title so the right expert can be assigned to best assist? If you are unsure you might consider a title such as "C2000 Inverter Design Solutions". 

    Regards,

    Steve