Hello,
Trying to generate AUX file by means of utility included into BQWIZARD package, I get the following log. How to overcome this?
Thanks
Opening input .csv file : C:\Program Files\Texas Instruments\bqWizard 3\Data Logging Files\3cell_4.csv
Opening Chemistry file : 0403.chem
Prereading data
........................................................................................................................
.................................................
Preread is Complete
Final Discharge from T = 499.854 to 615.818 shows capacity of 1887 mA
Current measured for first discharge was = 976 mA for an error of 1.667 %
Compiling profile of data file
Processing cycle : 1
Unknown error
undefined method `<<' for nil:NilClass
Position =