Other Parts Discussed in Thread: UCC14141-Q1, UCC14341EVM-069
I am using the equations in the UCC14341-Q1's datasheet to calculate the value myself,
and I am using the UCC1434x-Q1_Calculator_V8.xlsx as reference for comparison.
But I don't quite understand the equations.

What does the ΔCOUT mean in these equations?
My guess is that it is the tolerance of the capacitor, but I can't get the same value as the calculator.
How do I get the correct value of RLIM_MAX_H, RLIM_MAX_L1 and RLIM_MAX_L2?
And in RDR Circuit Component Selection part,
in UCC14341-Q1 's datasheet RLIM1's equation is

but in the calculator the value of RLIM1 seems to be from the UCC14141-Q1 's equation.(RLIM1 value is chosen by Equation 10.)
so which equation should I use?