This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS51397A: solution comfirm

Part Number: TPS51397A
Other Parts Discussed in Thread: TPS51388

Hi

The platform used by customers is Raptor Lake (Embedded)

1. Below are the two architecture diagrams of TI. Which architecture is used for i5-1345UE?

2. Please give priority to providing the circled recommended model specifications

  • Hi, 3.3V/5V not depends on CPU but system interface, so need to review system configuration, if current requirements are below 8A, we recommend promote 51383 and 51386, if current requires >=10A, we recommend TPS51397A and also we are developing 12A device TPS51388(you can send email to us for more details if needed.

    item2: controller for high current requirements over 10A or 12A, for these three P/Ns, recommend promote tps51285 with low Iq.

    Yuchang