This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS51200: Worst case tolerance on VO

Part Number: TPS51200

Hi Team, 

I want to calculate the worst case total tolerance on VO.

In my circuit 1.39V with 1.6% tolerance is applied to VLDOIN. Half of same voltage is applied to REFIN input using two 10K resistors with 3% total tolerance.

These two tolerances causes a +/-21mV deviation in REFIN voltage itself.

VOSNS has +/-15mV tolerance, REFOUT voltage tolerance to VREFIN is +/-12mV, then total tolerance on VO is 48mV.

This actually violating the JEDEC standard "VTTREF – 40 mV < VTT < VTTREF + 40 mV".

Also max. recommended DC operating VTT voltage for DDR3 in my application ( IS46TR16640CL) is from 0.642V to 0.725V. But the calculated max. voltage on VO pin is 0.7423V which exceeding the max. rated value.

Please help to resolve this issue as soon as possible.

Thanks

Akhil