Need UCC21222-Q1 Iq or Isleep current when IC in disable mode Vdis=high.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I believe it is on page 8.
Hi Prahlad,
When the device is in disable mode, the inputs are held low. With INA and INB held low, the typical input supply quiescent current is 1.5mA and the typical output supply quiescent current is 1.0mA.
This can be found under section 6.9 in the datasheet for UCC21222-Q1.
Link to datasheet:
Hope this helps!
Hiroki