This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61033: Waveform and frequency of PFM

Part Number: TPS61033


Hi support team,
This is a question regarding PFM operation.

Is there a way to calculate the waveform and frequency of PFM under the following conditions?

VIN = 5.3V
VOUT= 5.5V
IOUT= 0.05A
L = 2.2μH

Is it best to check by experiment?

Regards,
Dice-K

  • Hi Dice, 

    We can check it on the bench, but at first we need to make sure the BOM.

    As I said in another thread, 2.2uH is not recommended for TPS61033, 0.47uH is better.

    And please also provide the output capacitance, this is still related to frequency in PFM. If you load current is lower than 1A, 2*22uF output capacitors is recommended, otherwise 4*22uF output capacitors is recommended.

    Regards,

    Nathan