Hello colleagues,
I am going to hold up a display backlight supply voltage during pulses. The main 12V will start to drop down and the only one deactivating will be the display internal backlight driver circuit leading to flicker.
TPS61089 working as a boost DCDC with the output voltage quite similar to the 12V rail nominal voltage. How is this chip going to act if I set this one to 11V for example so that it will be (nearly) invisible during the normal operation but will go to regulation in case of a drop. Is this possible? (stable running at lowest Fsw in PFM for example or stopping switching and just bypass)
Thanks,
Daria