Other Parts Discussed in Thread: LM74722-Q1
Hello team.
Does LM74720-Q1 support EMC-CS:CI210?
Best regards,
Kazuki Kuramochi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello team.
Does LM74720-Q1 support EMC-CS:CI210?
Best regards,
Kazuki Kuramochi
Hi Praveen,
Please refer following material's page 53 regarding detail of this standard.
http://emc.jaguarlandrover.com.edgesuite.net/docs/download/JLR-EMC-CS_v1.0_Amendment_4.pdf
Best regards,
Kazuki Kuramochi
Hi Kazuki,
Thanks for sharing the standard document. This test is the same as AC Super imposed test in ISO 16750-2.
Yes, LM74720-Q1 can rectify the 100kHz AC super imposed signal up to 100 kHz.
In case you want higher AC super imposed signal rectification support, you can consider using LM74722-Q1 which can support upto 200kHz.