Hi all,
I would like to ask you some questions about GPC tool.
Simple Guide to Chemical ID Selection Tool (GPC) (Rev. A)
My customer got a Log of Lead-Acid battery and updated to GPC tool.
However, an error occured.
The following is an errow message.
The following errors were reported by the calculation engine:
Accuracy Error: Deviation is so high that it is most likely due to anomaly in the data. Please check that data files have recomended format, units and test schedule * Warning: Max R deviation ratio can not be checked because discharge hr-rate is above 12. Hr rate = 21.0887965131344 * Warning: Max R deviation ratio can not be checked because discharge hr-rate is above 12. Hr rate = 21.0887965131344 * Warning: Max R deviation ratio can not be checked because discharge hr-rate is above 12. Hr rate = 21.0887965131344 * Warning: All IDs disqualified because of too high resistance deviation. No suitable ID selection available
So I have some questions.
1) Is there any item to specify the material of the battery?
I think there is an error because the battery is recognized as Li-ion and hr-rate is 12.
I think the battery material should be specified as lead acid battery and the Hr rate should be 20.
2)When using 2 batteries for serial connection, is there any problem to set as 2 for 'NumCellSeries' of config.txt?
I think an error occurred because I set 12 here.
Best Regards,
Ryusuke