This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS732: TPS73201DCQR output ripple

Part Number: TPS732


Hi

I am using TPS73201DCQR LDO.Input voltage is 3.3V and output voltage is 1.8V/200mA.When Resistor load.is connected It is observed that output drops below up to 1.72V and output ripple is arround 348mV            peak-peak.

Test snap of actual waveform as per below.

Kindly suggest to resolve it

Thanks

Ulhas mane