Hi,
As for the feedback reference voltage Vref, the data sheet states that Rfbt and Rfbb should be set so that the accuracy is ±1%. If the resistance value varies due to changes in resistance value accuracy and temperature characteristics, and the Vref error swings from ±1% to ±3~4%, what kind of problems may occur?
Thanks,
Conor