This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello
i have designed a negative 5V supply with the LM2776DBVR
as i read the datasheet i'm not sure what would be the best C FLY to chose ?
i chose 2 x 4.7uF ?
for the input / output i chose 10uF / 10uF (although the EVM has 2 x 10uF at the input)
i have attached the schematic please check if it is ok ?
Hi,
Please note that it is not possible to get exactly -5Vout from +5Vin due to the inherent losses in the Charge pump.
The schematic looks good. However, I would recommend to use a lower Cfly like 1uF with 10uF input & output capacitor.
Regards,
Febin