This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100: SoC jumps rfrom 7% to 100% to 0%

Part Number: BQ34Z100
Other Parts Discussed in Thread: , , , BQSTUDIO

Hello,

we use bq34z100 as battery management with LED display for a device of ours.

The battery we use has the following ratings: 3.635VDC/ 7Ah / 25.44Wh.

We now encounter the following problem:

Sometimes the SoC jumps from <10% (one LED) to 100%(4 LEDs), then after some time back to 0%(no LEDs). What causes this or wich settings do we have wrong?

Bellow I've attached some screenshots of our settings and the corresponding logfiles.

Registers:

Data Memory:

logfile:

logerrormon.xlsxbqstartlog0%mon.log