Hi there,
we are using TPSM846C24, some questions to consult.
1. could you please help review the SCH? Vin=5V, Vout =0.95V/20A and 1V/26A.
2. section 7.3.1 tells the min requirements for Cin and Cout value as well as ESR requirement for polymer caps.
For Ceramic caps, should we consider DC bias effect? Are the Cin=4x22u and Cout =4x47uF Nominal value or Effective Value? Same question when determining RC compensation by table1


3. Is it necessary to place a SMT test point on COPM pin (pin 9)? and why?
4. what can we do on designing if we want to observe Switching node waveform on oscilloscope?
5. our EN pin is contorlled by MCU, but would met the situation that EN pin is floated. Is there internal pull-down on this pins? or should we place an external resistor?
Thanks very much!