Other Parts Discussed in Thread: LMR38020-Q1
The datasheet of TPS54262QPWPRQ1 is not clear about the efficiency of the device when the input is 24V-27V. I do not want to assume what it is from the graph with 7V and 14V input.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The datasheet of TPS54262QPWPRQ1 is not clear about the efficiency of the device when the input is 24V-27V. I do not want to assume what it is from the graph with 7V and 14V input.
Hello,
We limited on data for this product and do not have this information available. For new designs, we recommend the LMR38020-Q1 for applications that require 60V or above with 2A load current. If your application has different requirements, I can suggest a device that is better suited for it.
Best regards,
Ridge
Unfortunately, we are already in the design verification phase using TPS54262QPWPRQ1. Is it correct that there is no Efficiency Graph for 24V input with 5V and 12V output? That you can't provide this information at all?
Hello,
Unfortunately we do not have the data that you are requesting. You can order the EVM and evaluate the device for your application conditions: https://www.ti.com/tool/TPS54262EVM
Best regards,
Ridge