Please reference issue, "Calculating L1 for TPS50601 using example"
The datasheet still seems to have this factor of 2 error in subsection 9.2.2.2 for the output inductor, L1, calculation.
Can anyone comment on why the output inductance calculates to twice what is given as the solution (5.4uH as apposed to 2.7uH) for this design example. I speculate the Kind refers to the ratio between PEAK ripple current (not PEAK to PEAK) and the RMS output current.
Regards