Other Parts Discussed in Thread: BQ25170
I have this square wave with 100ms period 50% duty cycle on ISET pin.
ISET has only a 1.8k resistor connected.
ISET2 is stable low (10k pulldown + powered down MCU giving 200mV on pin, ohmeter confirms 10k pulldown on pin). Shorting the pin to GND does not change behavior.
IN voltage is stable at 5.1V (USB powered). I have also tried with a USB3 and USB2 ports. Same bahavior.
Battery is LiPol chemistry and voltage is 3.7V.
I have tried with 2 different LiPol batteries and behavior is the same.
What's going on here...?
I also had a current regulation problem with a previous board revision. See thread: e2e.ti.com/.../bq24040-iset2-pulldown-value
Unfortunately, I was not able to take extra measurements to push this thread further.
Thank you for your assistance