Other Parts Discussed in Thread: UCC2894, , UCC2897A, UCC28951
Hello teams,
I would like to design a offline power supply using forward converter topology.
The specifications are as follows
Input voltage: 280V to 330V
Output voltage: 100V
Power rating: 400W
Topology : Flyback or Forward
I checked "Power Management Guid 2018(Power Management Guide 2018 (Rev. R) (ti.com))", the guide said UCC2891~UCC2894 and UCC2897 can use typcal power range between 50 to 300W.
Can I use these IC for the above condition power supply?
Thanks and Regards
Tomohiro Yoshimura